2023-03-19 9:47 AM
I have installed the STM32CubeIDE 1.12.0 from the STM32 official website onto my Arch Linux laptop but when i try to launch it, it closes and reports an error after the splash screen.
I have searched on pacman (the arch package manager) for stm32cubeide too, but they are having the same error too. See the comments section on https://aur.archlinux.org/packages/stm32cubeide
Here is the error:
[ri@r Desktop]$ /opt/st/stm32cubeide_1.12.0/stm32cubeide_wayland
SWT WebKitGDBus: error creating DBus server Error binding to address (GUnixSocketAddress): No such file or directory
SWT WebKit: error initializing DBus server, dBusServer == 0
(STM32CubeIDE:9473): GLib-GIO-CRITICAL **: 16:40:15.499: g_dbus_server_get_client_address: assertion 'G_IS_DBUS_SERVER (server)' failed
#
# A fatal error has been detected by the Java Runtime Environment:
#
# SIGSEGV (0xb) at pc=0x00007fd88683ed16, pid=9473, tid=9474
#
# JRE version: OpenJDK Runtime Environment Temurin-11.0.17+8 (11.0.17+8) (build 11.0.17+8)
# Java VM: OpenJDK 64-Bit Server VM Temurin-11.0.17+8 (11.0.17+8, mixed mode, tiered, compressed oops, g1 gc, linux-amd64)
# Problematic frame:
# C [libswt-gtk-4950r5.so+0x3ed16] Java_org_eclipse_swt_internal_C_strlen+0xf
#
# Core dump will be written. Default location: Core dumps may be processed with "/usr/lib/systemd/systemd-coredump %P %u %g %s %t %c %h" (or dumping to /home/richard/Desktop/core.9473)
#
# An error report file with more information is saved as:
# /home/r/Desktop/hs_err_pid9473.log
Compiled method (nm) 9481 5616 n 0 org.eclipse.swt.internal.C::strlen (native)
total in heap [0x00007fd917d3c190,0x00007fd917d3c530] = 928
relocation [0x00007fd917d3c308,0x00007fd917d3c338] = 48
main code [0x00007fd917d3c340,0x00007fd917d3c528] = 488
oops [0x00007fd917d3c528,0x00007fd917d3c530] = 8
Compiled method (nm) 9486 5616 n 0 org.eclipse.swt.internal.C::strlen (native)
total in heap [0x00007fd917d3c190,0x00007fd917d3c530] = 928
relocation [0x00007fd917d3c308,0x00007fd917d3c338] = 48
main code [0x00007fd917d3c340,0x00007fd917d3c528] = 488
oops [0x00007fd917d3c528,0x00007fd917d3c530] = 8
#
# If you would like to submit a bug report, please visit:
# https://github.com/adoptium/adoptium-support/issues
# The crash happened outside the Java Virtual Machine in native code.
# See problematic frame for where to report the bug.
#
And the error report file is attached below.
2023-04-10 11:55 PM
Update from me on my Arch system:
Installing webkitgtk-6.0 (https://archlinux.org/packages/extra/x86_64/webkitgtk-6.0/) fixed the issue for me.
2023-04-11 7:44 AM
Installing the webkitgtk-6.0 package solved this issue for me on Arch.
2023-04-11 11:55 AM
The flatpak worked for Manjaro on my PC. None of the other work-arounds did.
2023-04-15 2:20 AM
I did it - but same problem, always crashes with the same error
Tumbleweed is too up-to-date for CubeIDE...
Waiting the next release and back on Windows :(
2023-04-15 10:54 AM
Or, much easier, switch back to STM32CubeIDE 1.11.x and everything will be ok.
2023-04-15 12:07 PM
Or, even better than that, toss that Eclipse-based STM32CubeIDE out the window, and use STM32CubeMX to generate code for use with Visual Studio Code or any IDE of your choosing.
2023-05-01 9:32 AM
Having the identical error on Fedora 38 using both the generic install and the RPM. I have webkit2gtk4.1 installed and get the same dump
2023-05-02 2:39 AM
Have it installed, does not work for me. Ubunutu Lunar 23.04
2023-05-04 7:29 AM
Update on this (with some solutions i found in the AUR comments / forum):
The issue is indeed in an incompatibility in webkit2gtk and eclipse. In an earlier post i said that installing webkitgtk-6.0 solved the issue, seems like it didn't.
But i have found a new solution which is removing webkit2gtk from your system (has to be done with pacman -Rdd otherwise cubeide will be removed as well). This breaks browser functionality in eclipse (which i don't really know what its supposed to be and have probably never used, so yea i'm fine with that). Someone else mentioned swapping webkit2gtk for chromium, which i guess could work, but i didn't bother trying. If you're interested in this you can probably find the comment (which also contained a link) in the comments of the AUR package.
2023-05-08 6:57 PM
Hello,
I want to start working with STM32WB55 micros.
Some time ago, with much trial-and-error, I installed STM32CubeIDE V1.8.0 on to my Suse-tumbleweed computer. It mostly works well (ask me for details if you want to know more). This installation type DOES NOT allow updates.
I downloaded STMCubeIDE V1.12.1 (generic linux), and installed it the same manner as above. It installs without complaining. But it does NOT run - it seems to start okay, prompts me for the "workspace", but shortly after java dies...
My java version is:-
openjdk 17.0.7 2023-04-18
OpenJDK Runtime Environment (build 17.0.7+0-suse-1.1-x8664)
OpenJDK 64-Bit Server VM (build 17.0.7+0-suse-1.1-x8664, mixed mode, sharing)
My STM32CubeIDE V1.8.0 still works as it did.
Can anyone help me?
Thanking you
Pedro