2023-08-08 9:21 PM
Hi,
While flashing code in STM32G474VBT6, I am getting below error. After reinstalling cube ide and cube programmer, same error continues.
STMicroelectronics ST-LINK GDB server. Version 7.4.0
Copyright (c) 2023, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
-------------------------------------------------------------------
STM32CubeProgrammer v2.14.0
-------------------------------------------------------------------
Log output file: C:\Users\NIKHIL~1\AppData\Local\Temp\STM32CubeProgrammer_a02888.log
ST-LINK SN : 68005200040000363036544E
ST-LINK FW : V2J42S7
Board : --
Voltage : 3.26V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x469
Revision ID : Rev X
Device name : STM32G47x/G48x
Flash size : 128 KBytes
Device type : MCU
Device CPU : Cortex-M4
BL Version : 0xD5
Debug in Low Power mode enabled
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a02888.srec
File : ST-LINK_GDB_server_a02888.srec
Size : 73.29 KB
Address : 0x08000000
Erasing memory corresponding to segment 0:
Error: Operation exceeds memory limits
Error: failed to erase memory
Encountered Error when opening C:\ST\STM32CubeIDE_1.13.1\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.1.0.202305091550\tools\bin\STM32_Programmer_CLI.exe.
Error in STM32CubeProgrammer
Shutting down...
Exit.
Can anyone help me to get solution?
Thanks
Nikhil
Solved! Go to Solution.
2023-08-08 10:27 PM - edited 2023-08-08 10:28 PM
I just installed STM32CubeIDE v1.13.1 and got the same "failed to execute MI command" error.
But the error does not occur with IDE v1.12.1 (since it's the same project).
I'm using IDE 1.12.1 because there have been several reports of BUGs with version 1.13, and I've only just installed this version in a virtual machine to test it, but I shouldn't use this version for now, version 1.12.1 already suits my projects at the moment.
2023-08-08 9:26 PM
I remember something similar happening, which only the ST-link utility was able to resolve by performing a complete FLASH erase.
2023-08-08 9:48 PM
2023-08-08 10:07 PM
I found this tip:
Other tips can be found with these keywords:
https://www.google.com/search?q=stm32cubeide+error+failed+to+execute+MI+command
2023-08-08 10:27 PM - edited 2023-08-08 10:28 PM
I just installed STM32CubeIDE v1.13.1 and got the same "failed to execute MI command" error.
But the error does not occur with IDE v1.12.1 (since it's the same project).
I'm using IDE 1.12.1 because there have been several reports of BUGs with version 1.13, and I've only just installed this version in a virtual machine to test it, but I shouldn't use this version for now, version 1.12.1 already suits my projects at the moment.
2023-08-08 10:49 PM
The error stopped occurring after selecting the ST-Link frequency from Auto to 8000kHz. There may be some ST-Link speed identification failure.
2023-08-08 10:54 PM
I disabled firmware verification, but I noticed that leaving 8000kHz in IDE 1.13.1 caused a firmware error. IDE version 1.12.1 identifies the frequency of 4000kHz for ST-link in AUTO mode.
2023-08-08 11:18 PM
I enabled firmware verification but I noticed leaving 1000kHz in IDE 1.13.1 stops with MI error.
2023-08-09 3:13 AM
Hi @RhSilicon ,
I uninstalled STM32CubeIde 1.13.1 and installed STM32CubeIde 1.12.0. Now it is working fine.
There may be some issue with 1.13.1.
Thanks for your help.
Regards,
Nikhil
2023-08-10 3:45 AM
I have the same issue 1.12.1 works but 1.13.1 doesn't