cancel
Showing results for 
Search instead for 
Did you mean: 

Encountered Error when opening STM32_Programmer_CLI.exe

dwJavad
Associate II

Hi! I'm trying to flash a STM32H723ZG with STM32CubeIDE 1.14.0 and ST-LINK V2

and use OSPI peripheral to communicate with the W25Q256 external flash as QSPI

and I have this error:

(I have tried all the suggestions given in the community to solve this problem, but I still haven't got any results.

The only way I could get the result was using STMcubeIDE version 0.4.

Do you have any suggestion to fix this problem in higher versions? Thank you)

 

ST-LINK FW : V2J44S7

Board : --

Voltage : 1.58V

JTAG freq : 9000 KHz

Connect mode: Under Reset

Reset mode : Hardware reset

Device ID : 0x483

Revision ID : Rev Z

Device name : STM32H72x/STM32H73x

Flash size : 1 MBytes

Device type : MCU

Device CPU : Cortex-M7

BL Version : 0x93

 

 

 

Memory Programming ...

Opening and parsing file: ST-LINK_GDB_server_a03076.srec

File : ST-LINK_GDB_server_a03076.srec

Size : 195.92 KB

Address : 0x08000000

 

 

Erasing memory corresponding to segment 0:

Erasing internal memory sector 0

Erasing memory corresponding to segment 1:

Erasing external memory sectors [0 1]

Download in Progress:

 

 

Error: failed to download Segment[0]

Error: failed to download the File

Encountered Error when opening C:\ST\STM32CubeIDE_1.14.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.1.100.202311100844\tools\bin\STM32_Programmer_CLI.exe

Error in STM32CubeProgrammer

Shutting down...

Exit.

18 REPLIES 18
Sbag
Associate II

I use the log file to see what is happening in detail

This is the output 

STMicroelectronics ST-LINK GDB server. Version 7.7.0

Copyright (c) 2024, STMicroelectronics. All rights reserved.

 

Starting server with the following options:

Persistent Mode : Disabled

LogFile Name : C:\Users\user\STM32CubeIDE\workspace_1.15.0\BLINKY\Debug\st-link_gdbserver_log.txt

Logging Level : 31

Listen Port Number : 61236

Status Refresh Delay : 15s

Verbose Mode : Enabled

SWD Debug : Enabled

 

COM frequency = 950 kHz

Target connection mode: Attach

Reading ROM table for AP 0 @0xe00fffd0

Hardware watchpoint supported by the target

ST-LINK Firmware version : V2J45S7

Device ID: 0x410

PC: 0x1

ST-LINK device status: RUN_MODE

ST-LINK detects target voltage = 3.28 V

ST-LINK device status: RUN_MODE

Stm32Device, pollAndNotify running...

ST-LINK device initialization OK

SwvSrv state change: 0 -> 1

Waiting for debugger connection...

Waiting for connection on port 61236...

Waiting for connection on port 61237...

Accepted connection on port 61236...

Debugger connected

Waiting for debugger connection...

Waiting for connection on port 61236...

GDB session thread running

GdbSessionManager, session started: 1

Try halt...

ST-LINK device status: HALT_MODE

Accepted connection on port 61236...

Debugger connected

Waiting for debugger connection...

Waiting for connection on port 61236...

GDB session thread running

GdbSessionManager, session started: 2

Enter STM32_SystemReset() function

Enter STM32_InitAfterReset() function

NVIC_DFSR_REG = 0x00000008

NVIC_CFGFSR_REG = 0x00000000

Stm32Device, closeDevice() entry

GDB session, device event: 5

GDB session, device event: 5

Stm32Device, pollAndNotify stopped

Stm32Device, closeDevice() exit

------ Switching to STM32CubeProgrammer -----

Encountered Error when opening C:\Program Files (x86)\STM32CubeIDE_1.15.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.1.201.202404072231\tools\bin\STM32_Programmer_CLI.exe

------ Switching context -----

Error in STM32CubeProgrammer

GDB session terminated: Client connection lost

GdbSessionManager, session terminated: 1

GDB session terminated: Client connection lost

GdbSessionManager, session terminated: 2

GdbSrv, last session terminated, signal dispose

Stopping port 61236

Received stop for port 61236, not accepting new connections.

GdbSrv, deInit entry.

Shutting down...

GdbSessionManager, deInit entry.

GDB session disposed: 2

GDB session disposed: 1

GdbSessionManager, deInit exit

SwvSrv deInit entry

Stopping port 61237

Stopping port 61236

Received stop for port 61237, not accepting new connections.

SwvSrv deInit exit

Stm32Device, closeDevice() entry

Stm32Device, closeDevice() exit

Stm32Device, deInit success

GdbSrv, deInit exit.

Exit.

 

The funny thing is I can upload the hex file from STM32CubeIDE using Stm32programmer as well as ST_LINK utility. But not STM32CubeIDE.

So there is no issue with ST-Link V2 (Clone?) or the Bluepill board. So this is definitely the IDE issue.

 

 

Sbag
Associate II

I have had similar problem with latest MPLAB for PIC ics with Pickit3.5 @ $25/- Vs ST-Link V2 @$2/-  

Lastest version will not connect with pickit. After banging my head for over a week , I had to uninstall clean various folders and registry and install a previous version. With each try it showed signs of life. finally installed 4 versions back. It was nightmare each operation taking almost 2 to 3 hours. Now it is working nicely. These companies deliberately discontinue support of older well tried debuggers for their much costlier new products. There also the pics could be programmed using their old standalone utility 

I am beginning to think, it is the same issue here too. STM may have silently withdrawn support for these cheap debuggers. Like the other one, I am able to program using standalone st-link utility which seems to be much better with comparison of file and device memory. The advantage of IDE for debugging is lost. May be it will work with an old version of Stm32CudeIDE too. 

In my case even openCD doesn't work. on CubeIDE. 

 

 [I could upload the code by changing the plugin.]

plugin ? pls explain. 

Pavel A.
Evangelist III

Encountered Error when opening C:\ST\STM32CubeIDE_1.14.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.1.100.202311100844\tools\bin\STM32_Programmer_CLI.exe

This error message is misleading. It suggests that STM32_Programmer_CLI.exe is not found or could not run.

In fact there was a runtime error, caused by external loader(?)

@STTwo-32 @Imen.D 

Besides fixing the root cause, suggest to change the message. Instead or "opening" - "executing" or like that.

 

AndersRasmussen
Associate

Any updates on this? We are experiencing what seems like the same issue as above.
We have tried uninstalling all existing STM software and reinstalled only the newest tools. Updated windows to the newest version as of 2024-07-10 (Windows10, version 10.0.19045, build 19045).
We are able to program the device using STM32CubeProgrammer but not using the STM_Programmer_cli.exe from CubeIDE.

@AndersRasmussen 
I've been stuck for a few days now and despite all my research and attempts, nothing seems to have solved the problem. I've also uninstalled and reinstalled all the ST tools but nothing works. I'm using Windows 11 but I've never had any problems.

Boris19_1-1724259200195.png

I can load my program with the .bin from STM32CubeProgrammer but I can't use the debugger from STM32CubeIDE 1.14 and 1.16.

Boris19_0-1724259131976.png


I hope that the ST teams find a solution... quickly.

I've solved the problem. It was a hardware short on the uP's NRST. I was misled by the fact that it worked once.

Sorry!

I don't understand how you solved the problem.

Can you explain more?

My hardware consists of several PCBs linked via connectors. On 2 of them there is a button that allows the uP to be reset. The aim is for the reset to be as accessible on the PCB containing the uP as it is on the one for the HMI.
In the end, the uP reset is connected as follows:

Boris19_0-1724661894336.png

When I press S5, the 0 ohm resistor R50 causes a short circuit on NRST.

According to the ST documentation, the pull-up resistor (Rpu, framed in red) for the NRST input is internal and fixed, so there is no need to add one.

I didn't understand why it didn't work because when I used STMCubeProgrammer I could load the program without any problem.

My intuition is that when using STMCubeIDE, at the time of debugging, the uP activates one of these outputs (framed in red) and pulls the transistor to ground. This causes the internal reset but it also causes the short-circuit due to my 0 ohm resistor R50. Conversely, when loading the program with STMCubeProgrammer, the uP does not activate the outputs because it uses the NJRST and this does not cause a short-circuit.

Boris19_1-1724662050329.png

I simply removed R50 and C50 and that solved the problem.

I hope my answer is clear enough.