2021-06-08 11:28 PM
Hello
I tried to use doxygen to a project folder from STM32CudeIDE but it does not generate the documentation. I also looked on how to use doxygen on eclipse but still no results.
Is there a way to use doxygen or any other tool for generating documentation on a project from STM32CubeIDE?
2021-06-09 7:18 AM
CubeIDE is Eclipse, whatever solution works for other Eclipses will work for CubeIDE.
2021-06-09 8:12 AM
You can run doxygen from the command line.
You must have a proper doxygen configuration file. You can generate the default one with 'doxygen -g' at the command line, then edit the resulting file.
In the configuration file, you have to tell it how/where to find the sources that it is supposed to document.
If you are missing the configuration file or doxygen cannot find the sources, it won't work.