2025-01-08 12:22 PM - edited 2025-01-09 01:02 AM
Hi,
In CubeIDE, new project, choosing STM32H755ZIT6 (the NUCLEO-H755ZI-Q), the board stops responding when turning off and on the power to the board. I have made a simple LED example with everything set to default with the addition of two user LEDs blinking - one controlled by M7 and one by M4 core. It works fine until you remove the USB and put it back in. Then ST-link cannot connect.
I have used the debug configuration from the application note:
STM32Cube Version: 1.17.0
CubeMX version: 6.13
Firmware package: H7 V1.12.1
Best regards Nikolaj
2025-01-08 11:54 PM - edited 2025-01-09 01:01 AM
Additional info: Everything works when using older software releases - I can power cycle the board as much as I like and the program runs every time with the LEDs blinking.
With these software releases, everything works:
STM32Cube Version: 1.16.1
CubeMX version: 6.12.1
Firmware package: H7 V1.11.2