2024-06-30 02:22 AM
Hello ST team,
It seems there is a bug on the latest revision CubeIDE (1.15.1) to use the DCMI function. The DCMI is able to active on the board Nucleo-H743ZI2 or Nucleo-H753ZI with STM32CubeIDE (1.14.1). But today, when I installed the latest revision (1.15.1), the it shows DCMI is an exclusive choice. As shown below, there is no pin conflict as all the pins have not been set up. Thx.
p.s. No issue on STM32CubeIDE 1.14.1. See below.
2024-06-30 03:04 AM
I mean 753 and 743 differ, you cant compare it, but yes every MX have own bugs and errata... is only wizard
2024-06-30 08:44 PM
yes I mean both boards are able to use the DCMI in CubeIDE 1.14.1, but cannot active on 1.15.1
2024-07-09 03:05 AM
Hello @Jiaming ,
Could you please share the .ioc file.
I'm not able to reproduce the issue using STM32CubeIDE 1.15.1 version as shown in the below figure.
Could you please try with latest versions of STM32CubeMX 6.12.0 or STM32CubeIDE 1.16.0 and let me know if the issue is solved or not?
Thank you for your contribution in STCommunity.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.