cancel
Showing results for 
Search instead for 
Did you mean: 

Data mismatch found at address 0x0C000004

Isko
Associate II

Whilst using the Trustzone examples given for the NUCLEO-WBA52cg Board

Tx_SecureLEDToggle_TrustZone

 RTC_TrustZone

CORTEXM_InterruptSwitch_TrustZone im encountering the error:

Error: Data mismatch found at address  0x0C000004 (byte = 0xF9 instead of 0x89)

Error: Download verification failed

Encountered Error when opening C:\ST\STM32CubeIDE_1.14.1\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubepError: Data mismatch found at address  0x0C000004 (byte = 0xF9 instead of 0x89)rogrammer.win32_2.1.100.202311100844\tools\bin\STM32_Programmer_CLI.exe

Error in STM32CubeProgrammer

Shutting down...

Exit.

When using the example 

  • GPIO_IOToggle_TrustZone

which was the first one I used, this error doesnt occur. Also the error only occurs when running the secure part of the example.

3 REPLIES 3
Ghofrane GSOURI
ST Employee

Hello @Isko 

First let me thank you for reporting.

I will internally check this issue and give you my feedback as soon as possible.

 

Thx

Ghofrane

Hello @Ghofrane GSOURI 

whilst checking for solutions to my problem I encountered another error which prevented the disabling of the TZEN option Bite.

 

08:57:17 : Error: Expected value for Option Byte "TZEN": 0x0, found: 0x1
08:57:17 : Error: Option Byte Programming failed Or modified by application after OB_LAUNCH

Isko
Associate II

Hello @Ghofrane GSOURI 

I wanted to ask if there are any news regarding my issue

regards 

Isko