2024-03-06 02:21 AM
Whilst using the Trustzone examples given for the NUCLEO-WBA52cg Board
Tx_SecureLEDToggle_TrustZone
RTC_TrustZone
CORTEXM_InterruptSwitch_TrustZone im encountering the error:
Error: Data mismatch found at address 0x0C000004 (byte = 0xF9 instead of 0x89)
Error: Download verification failed
Encountered Error when opening C:\ST\STM32CubeIDE_1.14.1\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubepError: Data mismatch found at address 0x0C000004 (byte = 0xF9 instead of 0x89)rogrammer.win32_2.1.100.202311100844\tools\bin\STM32_Programmer_CLI.exe
Error in STM32CubeProgrammer
Shutting down...
Exit.
When using the example
which was the first one I used, this error doesnt occur. Also the error only occurs when running the secure part of the example.
2024-03-06 06:11 AM
Hello @Isko
First let me thank you for reporting.
I will internally check this issue and give you my feedback as soon as possible.
Thx
Ghofrane
2024-03-11 12:58 AM
Hello @Ghofrane GSOURI
whilst checking for solutions to my problem I encountered another error which prevented the disabling of the TZEN option Bite.
08:57:17 : Error: Expected value for Option Byte "TZEN": 0x0, found: 0x1
08:57:17 : Error: Option Byte Programming failed Or modified by application after OB_LAUNCH
2024-03-14 02:41 AM