cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMx error

syedhashmiraza
Associate II

hello i downdload latest version but again this error will come when i press migrate or continue option after that iam updating my code in this code  goes to  error part. fix this problem.

 

Screenshot 2024-12-20 133438.png

25 REPLIES 25

@syedhashmiraza wrote:

yes i tried this one but still code not working


Share again the screenshot with that option.

And again check if you have C:/Users/Ciright/STM32Cube/Repository/STM32Cube_FW_F4_V1.28.1on your local disk drive --> please confirm that

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

iam facing same problem

 

syedhashmiraza_0-1734697910465.png

 

After checking that option, did you regenerate the code and click on "Migrate"?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

yes i did this but still error will come after  i genrate code 

SofLit
ST Employee

@Ghofrane GSOURI could help you on that.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Hello @syedhashmiraza 

Let's try this:

- Close the CubeMX.

- Go to C:\Users\XXXX    and delete .stm32cubemx

- Then Reopen the CubeMX 6.13.0 load your IOC.

THX

Ghofrane

mbarg.1
Associate III

This is NOT an ERROR.

It is a SWITCH between 2 options.

In xx.ioc editor,  project manager tab, check if "Use latest version" is checked.

If checked, every time you start edit an .ioc you can decide between 2 options, old version or new version

hello,When  i  generate and migrate  the code, my biometric code goes into the error part, but when I don't generate the code, my code runs properly. However, I need to integrate UART into it.

 
 

hello,When I integrate UART and generate and migrate  the code, my biometric code goes into the error part, but when I don't generate the code, my code runs properly. However, I need to integrate UART into it

 

@syedhashmiraza 

If the original question has been answered (posted in your first comment). Please accept as solution the comment that answered your question and open a new thread for the new request.

Thank you for your understanding.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.