2024-12-20 1:46 AM - last edited on 2024-12-20 2:12 AM by mƎALLEm
hello i downdload latest version but again this error will come when i press migrate or continue option after that iam updating my code in this code goes to error part. fix this problem.
2024-12-20 1:56 AM
Hello @syedhashmiraza
Could you please explain more about the error that you are facing?
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-12-20 1:59 AM
Hello,
Check if V1.28.1 is available in this path: C:/Users/<user name>/STM32Cube/Repository/
2024-12-20 2:33 AM
2024-12-20 2:48 AM
I mean check that you have STM32Cube_FW_F4_V1.28.1 folder at this drive location: C:/Users/Ciright/STM32Cube/Repository/
Otherwise, check the checkbox: "Use Default Firmware Location":
2024-12-20 3:00 AM
2024-12-20 3:05 AM - edited 2024-12-20 3:06 AM
You shared the same screenshot here.
I've already suggested, either:
1- to check if you have C:/Users/Ciright/STM32Cube/Repository/STM32Cube_FW_F4_V1.28.1 path on your drive.
or, check the checkbox: "Use Default Firmware Location" and regenerate the code. Normally CubeMx will download the missing package:
2-
2024-12-20 3:10 AM
i tried this one but still after i genarate code , shows error ?how can solve this error?
2024-12-20 3:29 AM
yes i tried this one but still code not working
2024-12-20 3:29 AM - edited 2024-12-20 3:29 AM
But I don't see from your shared screenshot you checked the option: "Use Default Firmware Location":