2024-04-10 6:58 AM
On Windows 11, the CubeIDE print dialog no longer provides an option to print only the selected text. Is there any way to restore this option?
Solved! Go to Solution.
2024-04-10 7:33 AM
I found a solution -- replace the totally worthless new Win11 print dialog with the legacy Win10 version, and the "Print Selection" option returns!
In Registry Editor (regedit.exe), browse to the following branch:
HKEY_CURRENT_USER\Software\Microsoft\Print\UnifiedPrintDialog:
Create a new REG_DWORD value named PreferLegacyPrintDialog
Set PreferLegacyPrintDialog data to 1.
Exit the Registry Editor.
2024-04-10 7:07 AM - edited 2024-04-10 7:08 AM
Might well be an Eclipse thing?
As a workaround, if you copy the selection & paste into Word it will retain the monospaced font and syntax highlighting; eg,
This has the advantage of giving you much better control over pagination, etc ...
2024-04-10 7:33 AM
I found a solution -- replace the totally worthless new Win11 print dialog with the legacy Win10 version, and the "Print Selection" option returns!
In Registry Editor (regedit.exe), browse to the following branch:
HKEY_CURRENT_USER\Software\Microsoft\Print\UnifiedPrintDialog:
Create a new REG_DWORD value named PreferLegacyPrintDialog
Set PreferLegacyPrintDialog data to 1.
Exit the Registry Editor.
2024-04-10 7:58 AM
Excellent!
I'll have to give that a go!
Please mark that as the solution so that others will find it.