2024-12-07 05:49 AM
Hello,
I've found an issue in STM32CubeIDE1.17.0.
When creating a project with USB Device used as a CDC Class and FreeRTOS an include is missing in app_freertos.c:
#include "usb_device.h"
The project runs properly, but a warning is issued at compile time:
implicit declaration of function 'MX_USB_Device_Init' [-Wimplicit-function-declaration] app_freertos.c /STM32G473CCU_FAN_CONTROLLER/Core/Src line 117 C/C++ Problem
As far as I remember, this issue was present in previous versions of STM32CubeIDE.
On the other side I don't remember having encountered this issue when using USB Host MSC class with FreeRTOS in projects targetting the STM32F429
Solved! Go to Solution.
2024-12-12 06:34 AM
Hi @zeboss49
Thank you for the clarification! An internal ticket is submitted 198619 to dedicated team to add the missing include.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-12-09 01:13 AM
Hi @zeboss49
I couldn't reproduce on my end. Would you attach IOC file ?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-12-09 04:55 AM
2024-12-12 06:34 AM
Hi @zeboss49
Thank you for the clarification! An internal ticket is submitted 198619 to dedicated team to add the missing include.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-12-15 05:19 AM
Hello,
I'm sorry for the late accept as solution.
I missed your answer.