cancel
Showing results for 
Search instead for 
Did you mean: 

CubeIDE closes itself

DBrug.712
Associate II

Hi, I'm going crazy over here because the stm32cubeIDE closes itself a few seconds after loading. Literally, I double-click on the icon, the program comes up, and sometimes after 5, 10, or 20 seconds, it closes itself. 

After cloasing a small window appears, I attach a picture of it. 

I have uninstalled all ST software I had on my PC, installed it again, installed the last versions and previous versions, updated to the last version of Win 10, but nothing works. Cube MX works fine, but the only issue is with this software. 

I have used the IDE on my PC for more than 3 years now with no issue. 

I searched for a log file with no luck, Does anybody know where it hides? Is there a log file?

Any help will be appreciated.

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
DBrug.712
Associate II

Ok, I got it working again.

Here is how I did it:

I uninstalled all STM software.

entered into the registry and wiped it from all keys that contain stm32cubeIDE and eclypse.

I reinstalled the IDE, and now it works.

 

View solution in original post

16 REPLIES 16
Issamos
Lead II

Hello @DBrug.712 .

Could you please add your OS to make the case as clear as possible.

Best regards.

II

DBrug.712
Associate II

Hi, my os is Windows 10 Home Single Language, version 22H2.

Thank you

Issamos
Lead II

Hello again and thank you for your feedback.

I think this post may help you.

Best regards.

II

DBrug.712
Associate II

Hi, colud catch the config, it's weey long so I attach a txt file. 

I found out that version 1.12.0 is working, I have no clue why version 1.13.1, that was running on my PC, refueses now.

I updated the IDE with the updater and it cloases itself in the new version.

DBrug.712
Associate II

Hi using stm32cubeidec.exe I got this log.

 

DBrug.712
Associate II

Ok, I got it working again.

Here is how I did it:

I uninstalled all STM software.

entered into the registry and wiped it from all keys that contain stm32cubeIDE and eclypse.

I reinstalled the IDE, and now it works.

 

Do you look in /etc?  I am not sure how to wipe registry.  Do you mind telling us the command you used?

 

@rick2399 in /etc, seriously? Windows is not Linux.

Ahmad M.Nejad
Associate III

I had the same problem.

solution:

1- Run as administrator STM32CubeMx.

2- Wait to complete installation of updates.

3- close STM32CubeMx and open STM32CubeIDE