2023-09-02 11:28 AM
Hi, I'm going crazy over here because the stm32cubeIDE closes itself a few seconds after loading. Literally, I double-click on the icon, the program comes up, and sometimes after 5, 10, or 20 seconds, it closes itself.
After cloasing a small window appears, I attach a picture of it.
I have uninstalled all ST software I had on my PC, installed it again, installed the last versions and previous versions, updated to the last version of Win 10, but nothing works. Cube MX works fine, but the only issue is with this software.
I have used the IDE on my PC for more than 3 years now with no issue.
I searched for a log file with no luck, Does anybody know where it hides? Is there a log file?
Any help will be appreciated.
Solved! Go to Solution.
2023-09-02 09:22 PM
Ok, I got it working again.
Here is how I did it:
I uninstalled all STM software.
entered into the registry and wiped it from all keys that contain stm32cubeIDE and eclypse.
I reinstalled the IDE, and now it works.
2023-09-02 11:49 AM
Hello @DBrug.712 .
Could you please add your OS to make the case as clear as possible.
Best regards.
II
2023-09-02 12:05 PM
Hi, my os is Windows 10 Home Single Language, version 22H2.
Thank you
2023-09-02 12:09 PM
2023-09-02 12:46 PM - edited 2023-09-02 12:48 PM
2023-09-02 02:45 PM
2023-09-02 09:22 PM
Ok, I got it working again.
Here is how I did it:
I uninstalled all STM software.
entered into the registry and wiped it from all keys that contain stm32cubeIDE and eclypse.
I reinstalled the IDE, and now it works.
2023-11-17 04:08 PM
Do you look in /etc? I am not sure how to wipe registry. Do you mind telling us the command you used?
2023-11-17 05:14 PM
@rick2399 in /etc, seriously? Windows is not Linux.
2024-01-25 01:45 AM
I had the same problem.
solution:
1- Run as administrator STM32CubeMx.
2- Wait to complete installation of updates.
3- close STM32CubeMx and open STM32CubeIDE