cancel
Showing results for 
Search instead for 
Did you mean: 

CubeIDE and Atollic installation on one machine?

Pavel A.
Evangelist III

Do they coexist peacefully on one system? Will CubeIDE overwrite any components such as OpenOCD or programmer, or standalone CubeMX data?

Thanks,

-- pa

1 ACCEPTED SOLUTION

Accepted Solutions
Cartu38 OpenDev
Lead II

Sounds no issue. If Windows (OS limitation) only one file association (.project / .cproject files) is supported. Latest installed IDE will take benefit of it. Here is only limitation I've faced myself.

View solution in original post

2 REPLIES 2
Cartu38 OpenDev
Lead II

Sounds no issue. If Windows (OS limitation) only one file association (.project / .cproject files) is supported. Latest installed IDE will take benefit of it. Here is only limitation I've faced myself.

Thank you