cancel
Showing results for 
Search instead for 
Did you mean: 

Could not verify ST device on STM32F407VGT6

untitled__666
Associate II

I have already updated my CubeIDE to the latest version 1.19.0 available on the official website. After writing the code with it, I attempted to download it to my F407VGT6 via STLink, but the download has never been successful. It always prompts "Could not verify ST device!" When I replaced one board with another, I was able to successfully download. The only difference between the two boards is that the silk-screening of the two VGT6s is slightly different. One has a small circle with "e3" inside and can be downloaded, while the one that cannot be downloaded has "e4" in the circle. I wonder if CubeIDE has not yet adapted to this chip. Has anyone encountered the same situation? I hope to get your solution!

16 REPLIES 16
Karl Yamashita
Principal

Your title suggests that STM32CubeIDE can't be downloaded from ST's site. Maybe change the title to "Could not verify ST device on STM32F407BGT6"

Are you using a development board or a custom board?

 

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.
CAN Jammer an open source CAN bus hacking tool
CANableV3 Open Source

AScha.3
Super User

Try connect with CubeProgrammer, to both, and show, what its telling (chip ID etc.).

If you feel a post has answered your question, please click "Accept as Solution".

Thank you. I have already modified the title. Yes, I'm using a custom board.

untitled__666
Associate II

untitled__666_0-1753288433185.png

OK, I have uploaded the screenshot of the fault code.


@untitled__666 wrote:

Yes, I'm using a custom board.


Then you need to give details of that board - we can't see it from here!

Please see: How to write your question to maximize your chances to find a solution.

 

Is it, perhaps, a so-called "Black Pill"?

If so, it might have a fake STM32...

 

Also, what ST-Link are you using?

How to recognize a genuine ST-LINK/V2 versus a cloned one.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

But actually, I don't think it's the problem of the board or the ST-LINK, because I have used the same ST-LINK and board for testing before. The only difference lies in the chip. When there is an "e3" silk-screen on the chip, it can be programmed; however, "e4" cannot.

e74a94ba025231be86e12a8af4a436b.jpg

untitled__666
Associate II

The same board, the same ST-Link programmer, but some chips just can't be programmed. Are the chips fake?!

TDK
Super User

Based on the screenshots, seems like the programmer is to blame, probably a fake. Show a picture of your programmer.

 

If you feel a post has answered your question, please click "Accept as Solution".

That soldering looks pretty bad. Doesn't look like it was soldered flowed. I would double check to be sure there are no shorts.

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.
CAN Jammer an open source CAN bus hacking tool
CANableV3 Open Source