2024-05-23 02:50 AM
Hi,
I had migrated my project from 1.14.1 to 1.15.1.
When I change PSC on TIM17 from 0 to 99 on IDE and regenerate the code.
The PSC value remains unchanged on tim.c, is this a bug or something I need to configure after migration?
This is really annoying that we need to check the parameter one by one to see if the change on IDE is generated to the source code.
Thanks for your help.
2024-05-23 08:10 AM - edited 2024-06-03 02:51 AM
Hello @Philip0107 ,
First let me thank you for posting and welcome to the ST Community.
For more investigation, I suggest please that you provide the ioc. File.
Thanks.
Mahmoud.
2024-05-23 08:37 PM
Thanks for your help
The ioc file is attached, it seems TIM17.Prescaler remains unchanged.
Philip
2024-05-24 02:52 AM
Hello @Philip0107 ,
I loaded the ioc file that you had attached on STM32CubeIDE 1.15.1, and I changed the Prescaler value of TIMER17, but the problem was not reproduced.
Thanks.
Mahmoud