cancel
Showing results for 
Search instead for 
Did you mean: 

Code generation issue after migrating from 1.14.1 to 1.15.1

Philip0107
Associate

 

Hi, 

I had migrated my project from 1.14.1 to 1.15.1.

When I change PSC on TIM17 from 0 to 99 on IDE and regenerate the code. 

The PSC value remains unchanged on tim.c, is this a bug or something I need to configure after migration?

This is really annoying that we need to check the parameter one by one to see if the change on IDE is generated to the source code.  

 

Philip0107_0-1716457510791.png

Philip0107_2-1716457678736.png

 

 

Thanks for your help.

3 REPLIES 3
Mahmoud Ben Romdhane
ST Employee

Hello @Philip0107 ,

First let me thank you for posting and welcome to the ST Community.

For more investigation, I suggest please that you provide the ioc. File.

Thanks.

Mahmoud.

Hi @Mahmoud Ben Romdhane , 

Thanks for your help :)

The ioc file is attached, it seems TIM17.Prescaler remains unchanged. 

Philip

Hello @Philip0107 ,

I loaded the ioc file that you had attached on STM32CubeIDE 1.15.1, and I changed the Prescaler value of TIMER17, but the problem was not reproduced.

MahmoudBenRomdhane_0-1716544160667.png

MahmoudBenRomdhane_1-1716544299375.png

Thanks.

Mahmoud