2024-07-31 05:01 AM
Hello,
I have successfully created a new cmake project in IDE 1.16. Everything I need works - the project is successfully compiled, the BIN file is successfully run in the MCU:
[ 97%] Building C object CMakeFiles/KubergCMAKE.dir/Drivers/STM32L0xx_HAL_Driver/Src/stm32l0xx_hal_uart_ex.c.obj
[100%] Linking C executable KubergCMAKE.elf
text data bss dec hex filename
48528 128 3376 52032 cb40 C:/Projekty/KubergCMAKE/Release/KubergCMAKE.elf
[100%] Built target KubergCMAKE
13:57:54 Build Finished. 0 errors, 0 warnings. (took 16s.631ms)
However, I am unable to compile the project from the command line window.
cmake --build Release
This command only succesfuly compile source files - 100% done, but when try to lining:
[100%] Linking C executable KubergCMAKE.elf
ends with this error:
.......
............
CMakeFiles/KubergCMAKE.dir/Drivers/STM32L0xx_HAL_Driver/Src/stm32l0xx_hal_uart_ex.c.obj : No such file or directory
collect2.exe: error: ld returned 1 exit status
make[2]: *** [CMakeFiles/KubergCMAKE.dir/build.make:639: KubergCMAKE.elf] Error 1
make[1]: *** [CMakeFiles/Makefile2:83: CMakeFiles/KubergCMAKE.dir/all] Error 2
Has anyone solved the same problem?
Thank You, Jan.
Solved! Go to Solution.
2024-08-01 04:25 AM
Hello @JKol
I suggest that you delete the Debug folder and rebuild the project with command line below:
cmake -DCMAKE_TOOLCHAIN_FILE=cubeide-gcc.cmake -S ./ -B Debug -GUnix -DCMAKE_BUILD_TYPE=Debug
cmake --build Debug --clean-first
It seems that the project was built using an older version of CubeIDE.
KR,
Souhaib
2024-07-31 09:00 AM
Hello @JKol ,
First let me thank you for posting!
I am not able to reproduce your issue in my side,
Could you add your project for further investigation.
Thx,
Souhaib
2024-07-31 10:25 PM
2024-08-01 04:25 AM
Hello @JKol
I suggest that you delete the Debug folder and rebuild the project with command line below:
cmake -DCMAKE_TOOLCHAIN_FILE=cubeide-gcc.cmake -S ./ -B Debug -GUnix -DCMAKE_BUILD_TYPE=Debug
cmake --build Debug --clean-first
It seems that the project was built using an older version of CubeIDE.
KR,
Souhaib
2024-08-01 04:46 AM
Hello Souhaib,
thanks a lot it's working :-). I only
1. added the path to compiler files to PATH variable:
c:\ST\STM32CubeIDE_1.13.2\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.win32_1.0.200.202406191623\tools\bin
2. changed cmake command:
cmake -DCMAKE_TOOLCHAIN_FILE=cubeide-gcc.cmake -S ./ -B Debug -G"Unix Makefiles" -DCMAKE_BUILD_TYPE=Debug
Best regards,
Jan.