cancel
Showing results for 
Search instead for 
Did you mean: 

Can't see RTOS tasks in debug window with JTrace IDE v1.2.1

JulienD
Senior

Hello,

When debugging with a JTrace connected, "Segger JLink" selected as debug probe, RTOSPlugin_FreeRTOS as RTOS variant , I can't see tasks in the debug window.

I'm using SWD.

Basically, that's a bug report (how to fill one).

I was thinking that cubeIDE would have been built on top of atollic adding new features. In fact, many features are missing in cubeIDE vs atollic. I'm a bit disappointed...

best regards.

Jullien

1 REPLY 1
Herve PIERROT
ST Employee

you are right, there are still few features missing vs previous Atollic TrueSTUDIO. And the FreeRTOS aware debugging is a major one that is in a good place in our ToDo list.

Could that be part of one the release in 2020... stay tune ;)