2023-11-23 10:40 AM
Hi, I want to use CAN interface to transfer integer data from one micro controller to another. I am using STM32F373C8 microcontrollers. Please brief me the hardware connection too, from google I understand following.
uC1-------------------uC2
CAN_H----------------CAN_H
CAN_L------------------CAN_L
GND----------------------GND
But in our case we have , CAN_Tx and CAN_Rx pins. I have also swapped the pins for transmission. The boards are placed quite close to each other. I have implemented the ChatGPT code, but it stucks some where in receiving. I am attaching my main file here. Please guide me as soon as possible
Solved! Go to Solution.
2023-11-23 11:55 AM - edited 2023-11-23 11:56 AM
Hello @Hassanfraz and welcome to the ST Community
I suggest you to use this exemple as a start for your project. This Can guide you on the configurations of your project.
PS: don't forget to take a look at the README file of the project.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-11-23 11:55 AM - edited 2023-11-23 11:56 AM
Hello @Hassanfraz and welcome to the ST Community
I suggest you to use this exemple as a start for your project. This Can guide you on the configurations of your project.
PS: don't forget to take a look at the README file of the project.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-11-24 06:46 AM
Please look at my question again, I think there is any hardware issue. I am not using any discovery board, I have two independent controllers and connections are as below.
uC1 ------------------ uC2
CAN_TX(A12)------------------CAN_RX(A11)
CAN_RX(A11)------------------CAN_TX(A12)
GND----------------------GND
Furthermore when i compile the software it struck in the transmit routine, on the following line.
if (HAL_CAN_AddTxMessage(&CanHandle, &TxHeader, TxData, &TxMailbox) != HAL_OK)
{
/* Transmission request Error */
Error_Handler();
}
Please guide me about the hardware as well.