C++ Project that creates C main file
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-03-10 11:31 PM
Hi,
If I create a C++ STM32CubeIDE project the main generated file is a C file (main.c) and I have to rename this to main.cpp every time I update pinmux, drivers, etc in order to call C++ functions. I think it's not an usual workflow but could anyone confirm this?
gaston
- Labels:
-
STM32CubeIDE
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-03-11 12:35 AM
Confirmed. You may add a BUG topic to this post if you like.
As a workaround, create your own .cpp files with a main_cpp() and call it from main() in a user code section.
hth
KnarfB
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-03-11 7:45 AM
"C++ project" means it has the C++ compiler step in addition to assembly and C. As if, if you add *.cpp files, it will handle them appropriately. Not sure if creating main.c is a bug or intended here.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-03-12 1:46 AM
I'm not sure if it's a bug or not but the MCUXpressoIDE works as expected. In this case If you create a C++ project the IDE generates a .cpp main file (MKE06Z4_Project.cpp). This is a natural workflow to me without doing workarounds.
gaston
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-03-12 8:57 AM
Please be sure, this is not a bug.
TL;DR Most of the ST libraries called by cube-generated code are plain C so it is just natural that the main.c is also a plain C file.
Perhaps the choice of the filenames main.c/main.h was not far-sighted, but it's too late to change. Many people already are used to this and will be upset if they change it.
OTOH integration of this C code with c++ is very easy (by design of c++).
For example, you can name your "main" cpp file like in MCUXpresso: "your_Project.cpp", change there main() to cpp_main(), and be done with it.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-03-13 4:41 AM
In this case it may be more appropriate to speak of 'very' nice-to-have feature.
The MCUXpresso libraries are also written entirely in plain C and if you create an MCUXpresso project in C++ you can call them from main.cpp without limitations. On the other hand, if you create a C project you won't be able to call libraries/functions written in C++.
Basically, creating a project in C++ should allow calls to C/C++ functions/libraries from main.cpp while a project created in plain C (main.c) will only allow calls to library functions written in plain C. I think no one will feel upset about this.
Despite creating a C++ project the STM32CubeIDE only generates a plain main.c instead of main.cpp. This makes it impossible to call C++ functions/libraries from main.c. I would have no problem renaming the file once but if I do multiple pinmux/peripherals updates they all generate a main.c and this workflow is no longer efficient at all.
gaston
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-03-13 10:41 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-03-13 10:49 AM
You're right, but looking at this from the Cube team POV, they would need to add a big feature - C++ code generation and all the templates; with all due validation and testing.
Is it really worth it?
C is not a broken C++, so there isn't anything to fix.
Maybe the old school, yep. I don't feel a slightest remorse from some C files in a C++ project. It works together cleanly, by design.
More to this... C++ is not 100% backward compatible with C (even "modern"), there are subtle incompatibilities. Compiling ST headers with C++ can cause at least a lot of warnings.
So for them adding C++ code generation is a non-nonsense effort with unclear reward.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-03-13 11:48 AM
@TDK No, you can't. In fact it is the opposite. Using extern C allows you to call C functions from C++.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-03-13 11:58 AM
@Pavel A.​ It is much easier than it seems. If you create a project in C++, the STM32CubeIDE simply has to generate a main file with the extension cpp instead of c. The rest of the code stays the same as in C and you don't need to do anything else. Then pinmux and peripheral updates modify the main.cpp file and voila. Everything flows. At least that's how MCUXpressoIDE does it. I don't know if other IDEs do the same, but it is true that many offer little support for C++.