2024-04-19 12:44 AM
Hi, for my STM32CubeIDE projects it would be convenient to have a macro whose value increases every time I compile the project; As if it were a counter of the times I pressed the build button, to be used as an ID to identify the specific build.
For example, in my code I would like to put a printf at the beginning that prints this number to understand which build the executable being executed belongs to.
On other IDEs there is a way to make a kind of pre-build script that is executed before compiling the project, the question is: is it possible to write a pre-build script also in STM32CubeIDE? If yes, how? In what programming language? Can I read and write C-MACROs from these scripts?
Thanks in advance
Solved! Go to Solution.
2024-04-19 9:42 AM
Yes I have one example, but not with CubeIDE.
I have "version.h" with all the usual major/minor numbers. Then I made a small c file. "getversion.c" :
//getversion.c
#include "Inc\version.h"
//#define FW_VERSION_SUFFIX -beta
//#define FW_VERSION_MAJOR 5
//..... etc
// #define STRINGIFY(s) #s
//#define VERSIONIZE(x, y, z, w) STRINGIFY(x) "." STRINGIFY(y) "." STRINGIFY(z) STRINGIFY(w)
//#define MY_FW_VERSION VERSIONIZE(FW_VERSION_MAJOR, FW_VERSION_MINOR, FW_VERSION_REVISION, FW_VERSION_SUFFIX)
MY_FW_VERSION
Then, in the pre-build script I run the compiler on getversion.c and get the actual version string like "5.2.0-beta":
iccarm --preprocess=ns $scripts_dir/getver.tmp $scripts_dir/getversion.c" > /dev/null
From that I generate various things to handle the build outputs.
But I don't modify the version automatically. Instead I edit version.h manually and assign the version number agreed with the customer.
You can use pre-build script to parse your previous version number and increment it before build.
2024-04-19 1:04 AM
Use the Pre-build or Post-build steps in your project properties under 'C/C++ Build > Settings > Build Steps' to call any script you want. Unfortunately there is no build in feature to support build numbers.
2024-04-19 1:16 AM - edited 2024-04-19 1:18 AM
I have a timestamp.c file:
/* Public variables ---------------------------------------------------------*/
const char build_date[] = __DATE__;
const char build_time[] = __TIME__;
So those strings can be printed as required - to show when the code was built.
I use this Pre-build step to ensure that the file is always recompiled:
Slight downside with this is that the timestamp file will always be rebuilt - even if no other files have changed.
I haven't found a better way in Eclipse to specify "include in every build" - like other tools have.
2024-04-19 1:27 AM - edited 2024-04-19 1:31 AM
You can do this in a usual "sh" or "dash" shell script. CubeIDE for Windows comes with set of common posix utilities. On Linux, OS/X you have the native bash and more.
Pre-build and post-build commands are set up per project, in the project settings.
> Can I read and write C-MACROs from these scripts?
C-MACRO? if you mean, preprocessing C-like expressions with defines and includes - yes, you can run the C compiler and produce preprocessor output.
2024-04-19 1:53 AM
I think that would suffer the same issue as my "timestamp": ie, the "build number" would get updated every time you press the 'Build' button - whether or not there was anything else in the rest of the project that would have been built?
The 'Pre-build' seems to come before the evaluation of whether there is actually anything that needs building?
2024-04-19 6:53 AM
@Pavel A. wrote:C-MACRO? if you mean, preprocessing C-like expressions with defines and includes - yes, you can run the C compiler and produce preprocessor output.
Ok, this is exactly what I need to do, but how do I start the compiler before compiling? Do you have any examples of how to do this?
2024-04-19 9:42 AM
Yes I have one example, but not with CubeIDE.
I have "version.h" with all the usual major/minor numbers. Then I made a small c file. "getversion.c" :
//getversion.c
#include "Inc\version.h"
//#define FW_VERSION_SUFFIX -beta
//#define FW_VERSION_MAJOR 5
//..... etc
// #define STRINGIFY(s) #s
//#define VERSIONIZE(x, y, z, w) STRINGIFY(x) "." STRINGIFY(y) "." STRINGIFY(z) STRINGIFY(w)
//#define MY_FW_VERSION VERSIONIZE(FW_VERSION_MAJOR, FW_VERSION_MINOR, FW_VERSION_REVISION, FW_VERSION_SUFFIX)
MY_FW_VERSION
Then, in the pre-build script I run the compiler on getversion.c and get the actual version string like "5.2.0-beta":
iccarm --preprocess=ns $scripts_dir/getver.tmp $scripts_dir/getversion.c" > /dev/null
From that I generate various things to handle the build outputs.
But I don't modify the version automatically. Instead I edit version.h manually and assign the version number agreed with the customer.
You can use pre-build script to parse your previous version number and increment it before build.
2024-07-18 6:11 AM
@Andrew Neil wrote:I think that would suffer the same issue as my "timestamp": ie, the "build number" would get updated every time you press the 'Build' button - whether or not there was anything else in the rest of the project that would have been built?
The 'Pre-build' seems to come before the evaluation of whether there is actually anything that needs building?
Emphasis added because this is precisely the situation I'm trying to solve. Starting a debug session, for example, automatically triggers an incremental build (this behavior can be changed, but I want it to do that). I don't especially want my build numbers incrementing just because I started a new debug session without changing any code.
I see that it's possible to change the arguments passed to make; is it possible to have user modifications to the makefile that will persist across clean/build cycles? I suspect make itself is clever enough to "do this only if you did that".