2021-05-18 11:42 AM
BUG ahead!
I created an assembler project in STM32CubeIDE with my own Makefile.
When setting a breakpoint in the assembler source view and start the debug session, the breakpoint is hit but it is displayed (the arrow) one line after the actual instruction where the BP was originally set to.
See attached example. Set a breakpoint on "resetHandler" and you will see that it shows one off.
Can anyone confirm, please? Will this Bug be fixed?
To reproduce:
2021-05-27 1:58 AM
Hello @chriskuku
I added the topic "STM32CubeIDE" to your post in order to increase its chance to be reviewed by our experts ( @Markus GIRDLAND )
Imen
2021-05-27 8:19 AM
Thanks a lot!
2021-05-28 1:46 AM
Hello there!
Thank you for tagging me, Imen!
I looked into the issue and from what I can see this issue only happens when a breakpoint is set at the program entry (either at the label “resetHandler�? or the first statement). Can you confirm?
My assumption is that GDB in this case will insert the breakpoint one instruction off since PC will already be at this location after reset.
If you want to debug from program entry my suggestion is to not using breakpoints but instead uncheck “Resume�? (Startup tab in the debug settings). Debugger should now connect to the state directly after reset.
If I'm misunderstanding anything then please let me know!
2021-05-29 1:36 PM
Thanks Markus.
I unchecked Resume in the Debug Configuration Tab. The program stops at rstHandler (Reset vector location). There is no explicit BP set there.
But I cannot step from there on.
2021-05-29 1:45 PM
I reverted to "Resume" ticked on again.
This time the first breakpoint is hit right on. Setting then another breakpoint further down (see screenshot) at "warm: nop" you can see the BP arrow being one off.
So the problem persists.
2021-06-01 2:33 AM
Any new findings? The issue is still there as you can see from the screen shot and it is not that it just happens at the Reset (rstHandler) entry point. I need to use breakpoints. How else should I be able to start my program and run it to a specific point of make use of all features that are possible with breakpoints (like conditions, counts, to name at least two)?
2021-06-01 4:40 AM
I have sent it to one of the developers to get their take on it. I'll get back to you as soon as I can.
2021-06-02 1:30 AM
Hello again,
I will relay what the developer told me here:
"I tried the �?simple.s�? provided in your attachment. I needed to remap the application code to 0x800000 in the linker file in order to get it to flash properly on a F4 device.
I can confirm the issue. A breakpoint on row 36 will in fact install the breakpoint one statement off. Not sure why GDB does this mapping. I will file a bug-report on this and try to investigate deeper."
As a last note in order to get as much information as possible in the bug-report, can you try to use instruction stepping and address breakpoints via the “Disassembly�?-view instead and see if this behavior changes for you?
2021-06-02 3:33 AM
Yes, I should have mentioned it in my OP. Indeed, when setting the BP in the disassembly view, it is set correctly and the arrow stops right on the set BP symbol.