2024-04-04 12:27 PM
STM32CubeIDE
Version: 1.14.1
STM32CubeMX - STM32 Device Configuration Tool
Version: 6.10.0-RC9
Build: 20231120-2037 (UTC)
OS: Linux (Mint 21)
I am trying to add support for FTP support using CubeIDE. In the Software Packs Component Selector, under Network NetXDuo> NetXDuo> there are several Addons that can be applied. One that I am currently using is Addons Web Server and that is working. However, I do not see a selection for FTP. I do find in the software packs repo for STM32H7 (version 3.2.0), in the Middlewares/ST/netxduo/addons folder another folder called ftp. This folder contains the nxd_ftp_server.c and nxd_ftp_server.h files I need to support ftp service. If I add those files to my project, in the same place the web addons are kept, when I regen the project the files I added are taken away. It seems like there should be several more options available in the Software Packs selection so CubeMx knows to add them or at least not take them away.
I guess for now, if have to put them in a safer location. A little annoying.
Solved! Go to Solution.
2024-11-27 12:37 AM
I worked out a FTP implementation for my project - I do have a 743 with usb memory key under filex - and it works with filezilla (read-write-delete both way) with some limitations: NO TLS support as now - that is ok in my project as my devices will not have port 21 accessible for outer world - code is alpha (proof of concept stage) and everybody who wants to work with me on this topics, welcome
2024-11-27 1:30 PM
Hey mbarg.1,
I found a solution to the problems with the AZRTOS Web Server and FTP Server. The main issue was the memory. I found a better memory assignment for all the tasks and got it working. As for the SD card, I made myself a board with an eMMC chip that gave me 8 GByte of storage.
It's the Kingston EMMC08G-MV28-01J10. It works very well on the NUCLEO-H753ZI board. The web server grabs files from the filesystem on the eMMC chip.
I just finished my upgraded "NUCLEO-MEM" board.
This board has the Kingston EMMC08G-MV28-01J10, an APS6408L-OBM-BA 8 MByte PSRAM, and an LXMS21ACMD-220 which is an UHF-RFID Impinj Monza4QT chip. I'm in the middle of testing it and hope it'll run OK.
The annoying issue with the STM32CubeMX code generation is that overwriting code still exists, but I mainly use VisualGDB from SysProgs for development, which is much better than STM32CubeIDE.
VisualGDB - Serious cross-platform support for Visual Studio
2025-03-12 2:12 AM - edited 2025-03-12 2:13 AM
upgrade to ver 3.3 - NetXDuo ver 6.4 and you have FTP - no demo or detailled instructions on how to use it - server and client but not both
2025-03-14 3:43 PM
Thanks for the info. I've had it running for quite some time now. I made a GitHub repo for whoever is interested:
intector/Test-XSPI: Working example for the use of XSPI on STM32H7R3L8H6H
It's like a starter project; I thought it'd save others time and frustration.
Great fleas have little fleas upon their backs to bite 'em,
And little fleas have lesser fleas, and so ad infinitum.
And the great fleas themselves, in turn, have greater fleas to go on;
While these again have greater still, and greater still, and so on.
Augustus De Morgan