assertion "REENT malloc succeeded" failed
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-07-23 9:31 AM
After upgrading CubeIDE from 1.3.0 to 1.6.1 and CubeMx from 5.6.1 to 6.2.1. I got this error:
assertion "REENT malloc succeeded" failed: file "/build/gnu-tools-for-stm32_9-2020-q2-update.20201001-1621/src/newlib/newlib/libc/time/lcltime.c", line 50
MCU: STM32H750
How to reproduce: Send the BLE message from mobile to BLE chip(QN9021). The BLE chip is connected to MCU via UART.
Any advice would be appreciated.
- Labels:
-
STM32CubeIDE
-
STM32H7 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-07-31 2:08 AM
@mattias norlander
I found the issue is happend while using new toolchain(gnu-tools-for-stm32_9-2020-q2-update...). If i switch back to the other installed toolchain (2018), it works fine. I saw you solved some toolchain issues, so could you help to check this issue?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-08-04 2:54 AM
Hi @JLee.32 ,
Latest STM32CubeIDE version is 1.7.0. Is initially reported issue still faced with this version?
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-08-09 12:41 AM
@Amel NASRI
Yes, the issue is still faced with 1.7.0.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-08-09 2:51 AM
Hi @JLee.32 ,
Thanks for your answer. In such case, I let our CubeIDE experts (@Markus GIRDLAND & @mattias norlander ) investigate the issue.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-08-10 12:48 AM
Hi @Markus GIRDLAND & @mattias norlander ,
I found the root cause is that localtime() is used in the task of freertos. localtime() calls malloc() which returns -1 due to _sbrk(). Using localtime_r() is one solution, but I'm wondering if we can overwrite the standard version of malloc? Please see this link. I add the following code at main.c and main.h, but it shows error. How should I do to overwrite the standard version of malloc?
~~~~~
/* Defining malloc/free should overwrite the standard versions provided by the compiler. /
void malloc (size_t size)
{
/* Call the FreeRTOS version of malloc. */
return pvPortMalloc( size );
}
void free (void* ptr)
{
/* Call the FreeRTOS version of free. */
vPortFree( ptr );
}
~~~~~
Regards,
Jimmy
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-08-16 3:21 AM
Hello Jimmy,
If you implement your own malloc it could be called before the application which might not be OK, depending on the application.
There were changes made to the _sbrk() (sysmem.c) in newer versions of STM32CubeIDE and the easiest way could be to generate a new project and copy over the updated version file with the _sbrk() function.
The application might also not be thread safe and you it's likely you would need to thread safe it, which you could do at the same time you update the _sbrk().
Also, it might be a bit unlikely, but it could be as simple as not using newlib nano. Even if that helps I would still recommend using an updated version of the _sbrk() function.