2020-07-25 2:44 AM
I have been developing boards with STM32G07x and STM32G07x G47x using ST-Link V2. I thought I would buy a better debug probe allowing more breakpoints and as a future investment in my development activities.
I am considering Segger J-Link Base, Plus or Ultra+ but it isn't clear to me whether STM32CubeIDE will use many of the features of these probes.
Examples
So I am wondering if anyone has any experience of using these Segger debugger probes and have found that they can use the advantages within STM32CubeIDE, or whether I would only gain any advantage of a more expensive Segger debugger by changing IDEs.
2020-07-25 5:09 AM
Critical paths on the CM0(+) cores do seem to limit the upper clocking rate. The ST-LINK/V3 clocks CM7 SWD at 15 MHz, up to 24 MHz supported/offered.
The cores have a finite number of breakpoints, hacks using Flash can be problematic and slow. If you really need a lot of breakpoints just use software ones rather than hardware, or use a breakpoint() subroutine, and step into code.
My personal view is that breakpoints so damage dynamic flow behaviours it is hard to see real benefit. If you need to single-step your own code in a dozen places you need to sharpen your static analysis. Real time telemetry and diagnostic output is much better at tracking dynamic flow and interaction/interplay within threads of operation.
Trace in the Cortex-M case is reconstructive in nature, primary use cases being profiling, and a small niche of how-the-heck-did-it-get-here problems.
ST has free Keil licenses for CM0(+) parts, debug/trace options there should be a lot richer
2020-07-28 7:17 AM
@Community member Thanks, I saw that there were Keil licences for CM0 and CM0+ but the G474 is M4 so Keil doesn't help for that.
I'm going to try one and see what difference it makes. I might move to Segger Embedded Studio eventually if it seems to be much of an advantage.