cancel
Showing results for 
Search instead for 
Did you mean: 

"No such file or directory" error even though the path is included

APilai
Associate

Hi,

I'm using the NUCLEO-H753ZI, with the STM32CubeIDE development tool (Version: 1.13.0, Build: 7399_20230707_0829 (UTC)).

While trying to build the project  - I'm countering the "No such file or directory" error even though the path is included!! see attached pictures.

The error sometimes happens, and sometimes not.

My project is Pure C - no C++ involved.

Before I moved to version 1.13.0 - it worked well on 1.12.0 (the error happened, but it was very rare).

Please assist - Thanks!

 

2 REPLIES 2
Stassen.C
ST Employee

Hello APilai,

Could you please send us your project? So that we can assist you.

Regards,

Stassen

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

APilai
Associate

Hi,

Solved the problem by including path - using the "Add/remove include path..." option:

APilai_0-1699798694388.png