2023-07-20 06:40 AM
Hi,
I'm using the NUCLEO-H753ZI, with the STM32CubeIDE development tool (Version: 1.13.0, Build: 7399_20230707_0829 (UTC)).
While trying to build the project - I'm countering the "No such file or directory" error even though the path is included!! see attached pictures.
The error sometimes happens, and sometimes not.
My project is Pure C - no C++ involved.
Before I moved to version 1.13.0 - it worked well on 1.12.0 (the error happened, but it was very rare).
Please assist - Thanks!
2023-07-21 01:49 AM
Hello APilai,
Could you please send us your project? So that we can assist you.
Regards,
Stassen
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-11-12 06:18 AM
Hi,
Solved the problem by including path - using the "Add/remove include path..." option: