cancel
Showing results for 
Search instead for 
Did you mean: 

ADC Triggered by Timer

B.Kaya
Associate II

Hello Team,

In my application using STM32G431KCU6 at 160MHz, I want to trigger ADC2 channel by TIM1 channel. 

I aim to read ADC value synchronously with 1.1kHz pwm signal. When I set up the CubeMX config, i can see that TIM1 trigger OutputCompareCallback function but i can not trigger ADC_ConvCpltCallback. Shared my ADC and TIM1 configuration below:

BKaya_0-1701065655338.pngBKaya_1-1701065679267.png

BKaya_2-1701065691737.png

BKaya_3-1701065745458.pngBKaya_4-1701065755994.png

Also I am confused about starting ADC on software because ADC is not continuous conversion mode. Should i start and stop ADC as below or any suggest? 

BKaya_5-1701066014358.png

My finalize code as below:

BKaya_0-1701071631917.png

 

Thanks for your help. 

Best Regards,

Basri.

 

1 ACCEPTED SOLUTION

Accepted Solutions
Mahmoud Ben Romdhane
ST Employee

Hello @B.Kaya,

First let me thank you for posting and welcome to the ST Community.

I advise you to consult this Post. It explains how to configure an STM32 Timer to trigger ADC conversions.

Thanks.

Mahmoud.

View solution in original post

1 REPLY 1
Mahmoud Ben Romdhane
ST Employee

Hello @B.Kaya,

First let me thank you for posting and welcome to the ST Community.

I advise you to consult this Post. It explains how to configure an STM32 Timer to trigger ADC conversions.

Thanks.

Mahmoud.