cancel
Showing results for 
Search instead for 
Did you mean: 

When will be the stm32mp157 fully supported bu cubemx ?

PMort.1
Associate II

Cannot select 8 bit wide bus for SDMMC controller (for use with e-mmc)

Cannot select USB:OTG_LS instead of USB_OTG_FS (to use 2 usb HS and the usb OTG LS togheter)

4 REPLIES 4
Khouloud ZEMMELI
ST Employee

​Hello @PMort.1​ ,

Thanks for your feedback,

For the second point : it's on going.

For the first point : Could you please share your ioc file ? because the 8 bits wide bus can be selected on my side.

Regards,

Khouloud                             

PMort.1
Associate II

Thanks for your reply

I have found the 8 bìt bus, it is only on the SDMMC2 controller; now i can select it (MMC 8 bits wide bus)

Regards

Paolo

​So no problem for the SDMMC ?

PMort.1
Associate II

Thanks

No i can choose from 1bit to 8bit for SDMMC2, without any problem.

Best regards

Paolo