2024-12-19 02:03 AM
Hello everybody,
i use "meta-st-x-linux-qt" with "meta-qt6" on STM32MP157
https://github.com/STMicroelectronics/meta-st-x-linux-qt
when I use "QMediaPlayer" to play an audio file it gives me the following error:
could not load multimedia backend "ffmpeg"
QtMultimedia is not currently supported on this platform or compiler.
Aborted (core dumped)
if I understand correctly, "ffmpeg" would be missing on my platform, how can I add it to yocto when generating it?
Thank you very much
Loupi
2025-01-27 06:31 AM
Hi,
have you used the "v2.0.0" branch of X-LINUX-QT meta layer?
Normally Qt6 Multimedia should be compiled as well, you can check if libQt6Multimedia.so is in usr/lib.
BR,
Philippe.