STM32 MPUs Software development tools

Ask questions and find answers on STM32 microprocessors software development tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 440 Views
  • 0 replies
  • 0 kudos

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 323 Views
  • 0 replies
  • 0 kudos

STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32Prog CLI and OTP Disply

Hi,i currently trying to interact via shellscript and stm32cubeprog cli with my stm32mp157 board.I can run and load tfa and than uboot. But when i want to read otp, my operations get stuck.What is the correct call for this?In my Script is use the fol...

STM32CubeIDE Serial Console in use

I am stuck at step 6 inhttps://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157C-DK2/Develop_on_Arm%C2%AE_Cortex%C2%AE-M4/Modify,_rebuild_and_reload_a_firmwareMPU Serial Console is operational, ethernet RJ45 also, and serial port ...

PeterL by Associate III
  • 5019 Views
  • 5 replies
  • 0 kudos

Resolved! I'm having trouble creating a project in STMCubeIDE 1.7.0. I'm trying to create the project in it's own directory, instead of the workspace directory. The process I am following is: (continued below)

- Create the directory for the project (C:\Project)- Create a New STM32 project- Select the processor and package- Setup STM32 project > Enter project name, for location enter project directory, select language and project type STM32Cube- Code Genera...

LThal.1 by Associate II
  • 4019 Views
  • 5 replies
  • 0 kudos

How to debug M4 in production mode?

I am trying to Debug m4 in production mode. M4 is not halted.I am getting an error "Failed to insert breakpoint".I can successfully debug in Engineering mode. but, I need to Debug in Production mode.Can you explain how to solve this issue?

JSIGA.1 by Associate II
  • 3386 Views
  • 6 replies
  • 0 kudos