cancel
Showing results for 
Search instead for 
Did you mean: 

The problem that CORE_CM4 Symbol is added but cannot be activated

HAPPYDAY
Associate II

When you create a project, CORE_CM4 symbol is added to properties by default.

However, if you look at stm32mp1xx_hal_rcc.h, the CORE_CM4 area is still disabled. Is it a bug? Can I ignore it and use it? Or please tell me how to solve it.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Cartu38 OpenDev
Lead III

Most probably same as: Issue with STM32CubeIDE file indexing on Dual Core STM32H7 Project.

If so, not a bug, not an issue, just a combination of common file indexing process and project structure choices.

View solution in original post

5 REPLIES 5
HAPPYDAY
Associate II

Related information is below.

IDE: STM32CubeIDE 1.6.1

Board : STM32MP157C-DK2

Image: Distribution Package (openstlinux-5.10-dunfell-mp1-21-03-31)

Firmware Package Version : STM32Cube FW_MP1 V1.4.0

Olivier GALLIEN
ST Employee

Hi @HAPPYDAY​ 

Did you check it impact compilation or if it can just be a graphical artifacts of CubeIDE ?

Thx,

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hi. Olivier GALLIEN

Doesn't seem to affect compilation (no error).

Then there should be no CubeIDE graphical artifacts, which is strange. please check.

Thank.

Cartu38 OpenDev
Lead III

Most probably same as: Issue with STM32CubeIDE file indexing on Dual Core STM32H7 Project.

If so, not a bug, not an issue, just a combination of common file indexing process and project structure choices.

Oh, I understand.

Thanks for the clear answer. It was helpful.