2022-09-16 03:47 AM
2022-09-16 08:43 AM
Hi @Gencay ,
1) please have a look to ES0438, there is a limitation for eMMC. DDR52 could be either use VDD=3.3V or 1.8V.
2) See previous, STPMIC1A is tailored for VDD=3.3V whereas STPMIC1B is for VDD=1.8V. It depend also on other external components IO voltages. VDD=3.3V is more usual unless absolutely needed.
3) See examples in AN5031 or STM32MP157F-EV1 as well as AN5089 or AN5260
Regards,
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'