Skip to main content
February 20, 2025
Solved

Starter package building configuration

Hi,

 

is it possible to know which is the Yocto configuration (manifest release, DISTRO and MACHINE used, other configurations, etc) used to generate the Starter Package of a board?

I think it could be a useful information for everyone. In fact I'm in a situation where the Starter package for STM32MP15 eco 6.0.0 does some operations that fails on an image built using Yocto (Distribution Package) at the same Ecosystem.

 

Thanks in advance

 

Mauro

This topic has been closed for replies.
Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
February 20, 2025

Hi @Legacy member ,

Starter Package for MP15 is generated with DISTRO=st-image-weston MACHINE=stm32mp1

Machine can be tuned to specific board : 

stm32mp1 Machine configuration for STM32MP1 microprocessor device boards
stm32mp13-disco Example of machine configuration for STM32MP13 discovery board (STM32MP135F-DK 
 

 

 in OP-TEE secure and system services boot mode on SDCard)
stm32mp15-disco Example of machine configuration for STM32MP1 discovery board (Only STM32MP157F-DK2 
 

 

 in OP-TEE system services only boot mode on SDCard)
stm32mp15-eval Example of machine configuration for STM32MP1 evaluation board (Only STM32MP157F-EV1 
 

 

 in OP-TEE system services only boot mode on SDCard)

What board are you using and what operation behave differently? 

Did you change DT somehow? 

Thanks

Olivier 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

2 replies

Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
February 20, 2025

Hi @Legacy member ,

Starter Package for MP15 is generated with DISTRO=st-image-weston MACHINE=stm32mp1

Machine can be tuned to specific board : 

stm32mp1 Machine configuration for STM32MP1 microprocessor device boards
stm32mp13-disco Example of machine configuration for STM32MP13 discovery board (STM32MP135F-DK 
 

 

 in OP-TEE secure and system services boot mode on SDCard)
stm32mp15-disco Example of machine configuration for STM32MP1 discovery board (Only STM32MP157F-DK2 
 

 

 in OP-TEE system services only boot mode on SDCard)
stm32mp15-eval Example of machine configuration for STM32MP1 evaluation board (Only STM32MP157F-EV1 
 

 

 in OP-TEE system services only boot mode on SDCard)

What board are you using and what operation behave differently? 

Did you change DT somehow? 

Thanks

Olivier 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
February 24, 2025

Hi @Olivier GALLIEN ,

 

Thank you for your answer, that points me to the right direction. More details following.

 


Starter Package for MP15 is generated with DISTRO=st-image-weston MACHINE=stm32mp1


I think there is a typo, I suppose you mean st-image-weston is the image and DISTRO is openstlinux-weston, right?

 


What board are you using and what operation behave differently? 

Did you change DT somehow? 


I used stm32mp15-disco MACHINE. I didn't change the DT.

Operation behaves differently is using TAs with optee: on Starter Package it works, on my build it doesn't work.

From table in your answer I found that optee is built in different ways depending on machines: "secure and system services" or "system services only". Digging in the (quite cumbersome) wiki I found that these two ways are called "profiles" (here more details), selected in Yocto by "optee" and "optemin" BOOTSCHEME_LABELS.

stm32mp1 MACHINE builds both profiles, but stm32mp15-disco MACHINE builds only "optemin" profile.
Adding BOOTSCHEME_LABELS += "optee" in local.conf allowed me to build a working image.

 

I would renew the invitation to put in the wiki how Starter Package is built (MACHINE, distro, image, exact repo tag, etc..): this information could be helpful and useful as in my case, and allows customers to build the exact packages provided by ST, validating their Yocto setup.

Thank you, regards
Mauro