cancel
Showing results for 
Search instead for 
Did you mean: 

Text editor

Olivier73
Associate II

Hi,

Does exist inside the Discovery kit with STM32MP135F board a text editor like nano or wim ?

And if not how can I install it ?

Thank you.

Olivier.

1 ACCEPTED SOLUTION

Accepted Solutions

Hi @Olivier73 

In that case, the utility vi is available by default.

Best regards,

--JM

View solution in original post

5 REPLIES 5

You're in the wrong forum: the STM32MP135F is an MPU - not an MCU.  <-- now moved.

 


@Olivier73 wrote:

a text editor like nano or wim ?


They're Linux things - so are you going to be running Linux on your STM32MP135F ?

If so, look at what's included in the Distro...

 

Yes it is on linux, but I don't now the name of the browser, I not an expert of linux.

Thanks for your help.

Jean-Marc B
ST Employee

Hi @Olivier73 

I currently use the Zile editor (see https://www.gnu.org/software/zile/) which is a lightweight Emacs clone.

It is available by default in the OpenSTLinux distribution.

From your board, just run the following command:

root@stm32mp1:~# apt-get update
root@stm32mp1:~# apt-get install zile

 

This is the example used in the wiki page dedicated to the Package repository service: https://wiki.st.com/stm32mpu/wiki/Package_repository_for_OpenSTLinux_distribution

 

Best regards

--JM

Hi Jean-Marc,

Thank you for your answer but for the moment I not yet connected on internet.

Merci

Hi @Olivier73 

In that case, the utility vi is available by default.

Best regards,

--JM