cancel
Showing results for 
Search instead for 
Did you mean: 

Networks settings

Olivier73
Associate II

Hi,

Each time I reboot my Discovery kit with STM32MP135F borad I lost the network (IP V4 address).

How can I set the IP address, Does exits somewhere a /etc/network/interface file ?

Thank you,

Olivier.

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
3 REPLIES 3

Does it not do DHCP?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

I want to use static IP address like 192.168.0.10.
so I send :

ifconfig eth0 192.16.0.10 netmask 255.255.255.0

then it works

but if i reboot the board I lost the network.

I would like to know wich file I need to setup.

Thank you