cancel
Showing results for 
Search instead for 
Did you mean: 

Can you recommend me a software for a login session?

DMårt
Lead

I have configure so my login session is done automatically. So once my STM32-OS starting at my STM32MP151 processor, then weston is up after few seconds.

OK! Good, but I want a login as well. Have anyone any recommendation of a software for a login session that works on STM32MP1 dev boards?

I have been trying with SDDM, without any success. It seems that it won't work.

kmscon will work...but...it's terminal based login only. Also kmscon using standard HDMI resolution, which is not good because if your text is to small, then you cannot change the resolution inside DRM.

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-Computer

STM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer
0 REPLIES 0