cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP157D-EV1 보드를 구입 하였습니다. ST-Link 를 연결하면 타겟보드가 연결�?� 안�?�다고 합니다.

HJoo
Associate

�?러메시지 입니다.

Can not connect to target!

Please select "Connect Under Reset" mode from Target->Settings menu and try again.

If you're trying to connect to a low frequency application , please select a lower SWD Frequency mode from Target->Settings menu.

​연결�?관한 좀�?� �?세한 정보는 알수없는지요?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
PatrickF
ST Employee

Hi,

i suggest that your start with https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-EV1

Unlike STM32 MCUs, the STM32 MPUs are not flashed using JTAG/SWD, so when using STM32CubeProgrammer you must use USB (and the board should be in serial/USB DFU mode).

JTAG/SWD is only used for debug purposes (e.g. with STM32CubeIDE).

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.