2021-03-23 4:30 PM
�?러메시지 입니다.
Can not connect to target!
Please select "Connect Under Reset" mode from Target->Settings menu and try again.
If you're trying to connect to a low frequency application , please select a lower SWD Frequency mode from Target->Settings menu.
연결�?관한 좀�?� �?세한 정보는 알수없는지요?
2021-03-25 12:21 AM
Hi,
i suggest that your start with https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-EV1
Unlike STM32 MCUs, the STM32 MPUs are not flashed using JTAG/SWD, so when using STM32CubeProgrammer you must use USB (and the board should be in serial/USB DFU mode).
JTAG/SWD is only used for debug purposes (e.g. with STM32CubeIDE).
Regards.