Skip to main content
hochul yoo
Associate III
March 18, 2021
Solved

How to customize openstlinux boot screen (psplash)

I am evaluate the STM32MP157C-DV2 board.

I have disabled the weston service by referring to the link below.

https://community.st.com/s/question/0D53W00000cSKmXSAW/disable-weston-autostart-in-stm32mp157cdv2

​

When boot with the weston service disabled

The two images below appear sequentially.

​

0693W000008xDuvQAE.png0693W000008xDv5QAE.pngI want to customize the boot screen to the image I want.

I found the above images in the path below.

layers/meta-st/meta-st-openstlinux/recipes-graphics/wayland/weston-init/

​

Although I did find the path of the default boot images,

I think it has nothing to do with weston-init because the weston service is inactive.

The psplash recipe exists in the path below.

layers/meta-st/meta-st-openstlinux/recipes-core/psplash/psplash-drm

layers/openembedded-core/meta/recipes-core/psplash

What recipe do I have to override in my custom layer to change the boot screen?

This topic has been closed for replies.
PatrickF
PatrickFBest answer
ST Employee
March 25, 2021

Hi,

first image is uBoot splash screen (splash.bin in bootfs I think)

second the Linux one

see section 7 in https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-DK2/Let%27s_start/Populate_the_target_and_boot_the_image

see also https://www.st.com/content/ccc/resource/training/technical/product_training/group1/ac/45/53/56/1f/0b/47/68/STM32MP1-Software-Platform_boot_BOOT/files/STM32MP1-Software-Platform_boot_BOOT.pdf/_jcr_content/translations/en.STM32MP1-Software-Platform_boot_BOOT.pdf

I'm not Linux nor Yocto expert, maybe this one could help:

https://www.youtube.com/watch?v=hqGA5Krk0mU with files in https://drive.google.com/drive/folders/1eHO37VljVpbTt-TBJFZ2-Yack5fZPj-v

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent

1 reply

PatrickF
PatrickFBest answer
ST Employee
March 25, 2021
In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent