2022-11-24 9:01 AM
Hi,
We are using SEEED studio 102110318 module which uses STM32MP157CAC3 processor. We want to know if there is any way we can keep processor pin PD13 pin to low state in suspend state. We want the pin to maintain low state while in sleep mode. We have added pullup on this pin in Hardware which is affecting one of our peripheral operation in sleep mode. For this reason we want this pin to be set low which will solve the issue. We do not have any other option to remove pullup in hardware as our device production is completed
Regards
Narendra Singh
2022-11-24 9:21 AM
Hi @kumar singh
If you are referring to HW STANDBY mode (as per Reference Manual) with VDDCORE in shutdown, there is no way to have a GPIO active in that state (as per HW, all GPIOs are in high-z during STANDBY as thr is no core supply).
I see no SW solution for that.
Few HW possible solution :
Regards.
2022-11-24 9:59 AM
Hi Patrick,
Thanks for your clarification. We were looking for SW fix if possible as our finished product is already delivered to client. Hence its difficult to do rework at this moment. Its a blunder we didn't test the use case before delivering. Now we are not left with any solution other than to remove pull up in hardware(pull up removal will solve our problem). Anyway, Thanks a lot.
Regards
Narendra Singh