2020-06-11 4:50 AM
Hi:
I have a MIPI LCD ,the driver IC is S6D7AA0X04,the LCD brief shows that the data lane is 4,and the pixels is (1280x800) less than 1366*768,if LCD data lane is configurable,Can I drive it with the STM32MP157C?
thanks�?
2020-06-11 5:25 AM
Hello,
It should work, with checking on your LCD that it should be set to use 2 data lanes and could support a bandwidth of 1Gbit/s per lane (required to support 1280x800 24bits 60fps).
2022-06-23 6:54 AM
Hello Patrick,
I have the same question for an MIPI LCD, 4 lanes with the MP1
it seems the LCD cannot be configured to 2 lanes with any pins
LCD chipset = HX8282-A/C / HX8696-A01
Resolution of 1024x600 16.7M and support colors
Tlpxm and Tlpxd are 50nsec Min and 75nsec max.
TTA-SUREs = 2xTlpxd
TTA-GETD = 5xTlpxd
TTA-GOD=4xTlpxd
How to check from the chipset or LCD datasheet it can support the timing ?