2021-09-29 1:47 AM
Hi All
I have disabled the second core to validate one of old product, which runs on single core,
and same application cpu usage i have seen is 90-95 %
and same application runs and does the same spi transaction, i am seeing the cpu usage is 57%
all constraint are same except the core
following is the top of stm32mp1
top - 04:18:53 up 37 min, 1 user, load average: 1.70, 1.65, 1.51
Tasks: 107 total, 4 running, 103 sleeping, 0 stopped, 0 zombie
%Cpu(s): 4.5 us, 93.4 sy, 0.0 ni, 1.5 id, 0.3 wa, 0.0 hi, 0.3 si, 0.0 st
9 root 20 0 0 0 0 S 2.3 0.0 0:05.56 ksoftirqd/0
78 root 20 0 0 0 0 I 1.6 0.0 0:03.88 kworker/0:2-pm
768 root 20 0 4556 1544 1204 R 1.0 0.2 0:01.27 top
612 root 20 0 113608 6668 4068 R 57.6 0.7 21:52.52 pxl
78 root 20 0 0 0 0 I 16.8 0.0 1:44.42 kworker/0:2-pm
63 root 20 0 0 0 0 S 8.2 0.0 2:43.77 spi1
62 root -51 0 0 0 0 S 7.4 0.0 2:30.84 irq/30-44005000
9137 root 20 0 0 0 0 I 2.4 0.0 0:01.96 kworker/0:0-pm
10 root 20 0 0 0 0 R 0.6 0.0 0:10.91 rcu_preempt
768 root 20 0 4556 1544 1204 R 0.6 0.2 0:18.68 top
9 root 20 0 0 0 0 R 0.3 0.0 0:10.92 ksoftirqd/0
what am observing , is that the SPI irq is running with very high priority -51, which makes our APP(pxl) deviates from cpu usage from 90 to 57,
is there any solution, to get pxl use cpu 90-95%
2021-09-29 2:13 AM
Hi @Ara.1 ,
Sorry it's not clear.
Do you mean that you application pxl is not working properly ?
CPU usage is not meaningful as such.
What was the old core performance ? ( mips, frequency )
Olivier
2021-09-29 2:36 AM
application $APP is working for the number of while (1){} ,
number of execution rate per sec are reduced when spi in action,
2021-09-29 2:58 AM
I have checked the drivers/spi/spi-stm32.c driver, while transfer spi
[ 78.789827] transfer of 4 bytes (4 data frames)
[ 78.794371] dma disabled
[ 78.796905] timeout set to 10 msecs
how to enable dma for SPI ?
2021-09-29 5:54 AM
if we increase the nice the normal thread
63 root 25 5 0 0 0 S 8.2 0.0 1:19.19 spi1
spi normal thread...
this brings back $APP normal.
root@mp1som:~# top
top - 02:54:47 up 17 min, 1 user, load average: 2.01, 1.99, 1.44
Tasks: 110 total, 3 running, 107 sleeping, 0 stopped, 0 zombie
%Cpu(s): 4.6 us, 93.8 sy, 0.0 ni, 1.0 id, 0.3 wa, 0.0 hi, 0.3 si, 0.0 st
MiB Mem : 935.4 total, 810.0 free, 47.7 used, 77.6 buff/cache
MiB Swap: 0.0 total, 0.0 free, 0.0 used. 852.2 avail Mem
PID USER PR NI VIRT RES SHR S %CPU %MEM TIME+ COMMAND
540 root 20 0 113636 6744 4176 R 64.7 0.7 10:56.47 pxl
62 root -51 0 0 0 0 S 12.1 0.0 1:57.49 irq/30-44005000
63 root 25 5 0 0 0 S 8.2 0.0 1:19.19 spi1
23 root 20 0 0 0 0 I 6.9 0.0 0:29.57 kworker/0:1-pm
3289 root 20 0 4556 1604 1264 R 1.0 0.2 0:03.61 top
2021-09-30 2:33 AM
Hi @Ara.1 ,
Ok you application doing while (1) it take all remaining CPU and is a good indicator of CPU taken by other threads.
Anyway I don't get you last status :
"if we increase the nice the normal thread"
What do you mean ? Can you rephrase ?
Does this mean point is close ?
Thx
Olivier