Skip to main content
Ozone
Principal
October 28, 2024
Solved

resources/documentation for getting started in CM4 application development on MP1 devices

  • October 28, 2024
  • 3 replies
  • 1063 views

While I got some experience with Cortex M devices - including several STM32 families - and Linux as host OS, I'm pretty new to asymmetrical dual-core systems like the STM32MP1 devices.
What sets them apart is the tight integration of both cores, and the ability to run realtime bare-metal applications in close cooperation with Linux as a host OS. Or so I think.

What I got already are the MP135-DK on the way, the OpenLinux Dev package installed and running, and a small user space application built. The CubeMP1 and CubeMP13 packages with the CM4 BSP, HAL, and very few examples.

And of course the MP1 datasheets/reference manuals, which I browsed.I think I have identified some of the important chapter, but I'm not yet through.

So, here my questions.

Since I haven't found any such thing yet, is there a single proper documentation of the API for synchronisation and communication between the CA7 and CM4 core ?
In particular, configuration of CM4 setting, code deployment (as the CM4 seems to execute from RAM only), and message/data transfer ?

Are there any example applications for this inter-operation available ? I haven't found any yet.

And finally, I very much prefer Segger ES as IDE/toolchain for the M4, instead of CubeIDE. And not only because I don't want just another 1+GByte vendor-specific IDE. Anybody using Segger Embedded Studio in this environment ?

Thank you !

This topic has been closed for replies.
Best answer by PatrickF

Hi @Ozone 

please note that STM32MP13x does not have Cortex-M4 coprocessor.

You should use STM32MP15x products to get a Cortex-M4 coprocessor (or STM32MP25x which has a Cortex-M33 coprocessor).

For more information on coprocessor usage, wiki provide plenty of details

maybe start with https://wiki.st.com/stm32mpu/wiki/Coprocessor_management_overview

Regards.

 

3 replies

Ozone
OzoneAuthor
Principal
November 5, 2024

> Since I haven't found any such thing yet, is there a single proper documentation of the API for synchronisation and communication between the CA7 and CM4 core ?

According to some example projects, this would be openAMP - to answer my own question.

 

PatrickF
PatrickFBest answer
ST Employee
November 6, 2024

Hi @Ozone 

please note that STM32MP13x does not have Cortex-M4 coprocessor.

You should use STM32MP15x products to get a Cortex-M4 coprocessor (or STM32MP25x which has a Cortex-M33 coprocessor).

For more information on coprocessor usage, wiki provide plenty of details

maybe start with https://wiki.st.com/stm32mpu/wiki/Coprocessor_management_overview

Regards.

 

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
Ozone
OzoneAuthor
Principal
November 6, 2024

> please note that STM32MP13x does not have Cortex-M4 coprocessor.

> You should use STM32MP15x products to get a Cortex-M4 coprocessor (or STM32MP25x which has a Cortex-M33 coprocessor).

You are right, that applies to the MP15x.
And since the discovery kits are relatively affordable, I got a MP135-DK and MP157-DK, thus the question remains valid for me.
I will definitely have a look at the wiki page, thanks.


Although, if I might add that here, the Cube packages for the MP157 CM-4 processor seem to be a mess.
BSP files and CMSIS folders missing in some variants, and a mixture of CubeIDE, SW4STM32 and Eclipse projects.
I will surely have some follow-up questions.