2023-08-22 1:50 PM
Hi,
I am trying to migrate my project (custom board using stm32mp153a and 256MB mem) from 4.1.0 to 5.0.0 but I am getting a panic when booting u-boot:
Board: MBfdd8 Var2.15 Rev.B-14
DRAM: 256 MiB
E/TC:0 tzc_it_handler:79 TZC permission failure
E/TC:0 dump_fail_filter:420 Permission violation on filter 0
E/TC:0 dump_fail_filter:425 Violation @0xcff09000, non-secure privileged write, AXI ID 480
M/TC: CPU : 0
M/TC: usr_sp : 0x00000000
M/TC: usr_lr : 0x00000000
M/TC: irq_spsr : 0x00000000
M/TC: irq_sp : 0x00000000
M/TC: irq_lr : 0x00000000
M/TC: fiq_spsr : 0x00000000
M/TC: fiq_sp : 0x00000000
M/TC: fiq_lr : 0x00000000
M/TC: svc_spsr : 0x00000000
M/TC: svc_sp : 0xcdef2ca0
M/TC: svc_lr : 0xcff0a2f0
M/TC: abt_spsr : 0x00000000
M/TC: abt_sp : 0x00000000
M/TC: abt_lr : 0x00000000
M/TC: und_spsr : 0x00000000
M/TC: und_sp : 0x00000000
M/TC: und_lr : 0x00000000
M/TC: pmcr : 0x41072000
E/TC:0 Panic
M/TC: CPU : 0
M/TC: usr_sp : 0x00000000
M/TC: usr_lr : 0x00000000
M/TC: irq_spsr : 0x00000000
M/TC: irq_sp : 0x00000000
M/TC: irq_lr : 0x00000000
M/TC: fiq_spsr : 0x00000000
M/TC: fiq_sp : 0x00000000
M/TC: fiq_lr : 0x00000000
M/TC: svc_spsr : 0x00000000
M/TC: svc_sp : 0xcdef2ca0
M/TC: svc_lr : 0xcff0a2f0
M/TC: abt_spsr : 0x00000000
M/TC: abt_sp : 0x00000000
M/TC: abt_lr : 0x00000000
M/TC: und_spsr : 0x00000000
M/TC: und_sp : 0x00000000
M/TC: und_lr : 0x00000000
M/TC: pmcr : 0x41072000
I am posting the full boot log as an attachment.
I am stuck any help is appreciated.
Solved! Go to Solution.
2024-08-12 5:34 PM
I am glad it helped at least one more person.
2024-08-13 1:59 AM - edited 2024-08-13 1:59 AM
Yes, but why does this working? @cfilipescu
optee@ce000000 {
reg = <0xce000000 0x2000000>;
no-map;
};
2024-08-13 9:04 AM
It changes the location of the optee in memory so that it is inside the 256MB