cancel
Showing results for 
Search instead for 
Did you mean: 

Multiple Endpoints on A7 and M4

YRink.1
Associate II

Hello,

iam trying to implement more or less the same example as with the virtualUARTs with multiple Endpoints just with the rpmsg_char driver and plain endpoints without virtualUART on M4 side. Iam struggling to get multiple Endpoints to work. One is working fine and the other is created as well. But i cant send and receive data through the second endpoint. Does anyone have an example with multiple endpoints with the rpmsg_char driver?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
ArnaudP
ST Employee

Hello,

The rpmsg_char is not compatible with the rpmsg virtio neither in ST or in kernel.org distribution. So I assume that you are using a specific Linux Kernel patch coming from Xilinx, right?

Xilinx has patched the kernel to be able to use the rpmsg_char. So no guaranty that this works with several endpoints and on another platform. Seems the same for the example, only one endpoint is created (charfd is a global variable).

So you have to understand the behavior of such implementation, as mentioned in my previous mail, a good entry point is to analyze the RPMsg exchanged by enabling the dynamic debug

echo -n 'file virtio_rpmsg_bus.c +p' > /sys/kernel/debug/dynamic_debug/control
echo -n 'file virtio_ring.c +p' > /sys/kernel/debug/dynamic_debug/control

View solution in original post

4 REPLIES 4
ArnaudP
ST Employee

Hello,

Could you detail your context, as the rpmsg_char is not supported in the ST distribution.

Do you back-port this series: https://patchwork.kernel.org/project/linux-remoteproc/list/?series=446305&state=%2A&archive=both ?

Be careful in this case to fix the Linux Local endpoint addresses to avoid that this address change, each time you open/close the /dev/rpmsgX.

On my side i tested using the OpenAMp TTY echo exemple ( so the virtualUARTs) , by disabling the rpmsg TTY on Linux side and it works well.

I would suggest you to enable the dynamic debug on Linux and enable rpmsg_virtio traces :

https://wiki.st.com/stm32mpu/wiki/Linux_RPMsg_framework_overview#How_to_trace_and_debug_the_framework

Theses traces print messages with source and destination addresses to help you to debug.

YRink.1
Associate II

Hello,

i enabled the rpmsg_char device via Yocto and with one endpoint its working fine for me but not with two. I tried to use fixed adresses not based on RPMSG_ADR_ANY. Still it only works for one endpoint. My usage of the rpmsg_char is based on the Xilinx example https://github.com/Xilinx/meta-openamp/blob/master/recipes-openamp/rpmsg-examples/rpmsg-echo-test/echo_test.c. The M4 creates the two "Channels" virtio0.rpmsg-openamp-demo-channel.-1.0 and virtio0.rpmsg-openamp-demo-channel.-1.1. Iam actually able to acess both it but with the virtio0.rpmsg-openamp-demo-channel.-1.1 i cant exchange data.

A part of my M4 code is attached.

ArnaudP
ST Employee

Hello,

The rpmsg_char is not compatible with the rpmsg virtio neither in ST or in kernel.org distribution. So I assume that you are using a specific Linux Kernel patch coming from Xilinx, right?

Xilinx has patched the kernel to be able to use the rpmsg_char. So no guaranty that this works with several endpoints and on another platform. Seems the same for the example, only one endpoint is created (charfd is a global variable).

So you have to understand the behavior of such implementation, as mentioned in my previous mail, a good entry point is to analyze the RPMsg exchanged by enabling the dynamic debug

echo -n 'file virtio_rpmsg_bus.c +p' > /sys/kernel/debug/dynamic_debug/control
echo -n 'file virtio_ring.c +p' > /sys/kernel/debug/dynamic_debug/control

ArnaudP
ST Employee

More of the discussion is available here : https://github.com/OpenAMP/open-amp/discussions/279