How to build a OpenSTLinux Distribution package image having multiple python versions?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2025-03-11 6:14 AM
I am new to building images using Yocto. I am working with an STM32MPU157F, which comes with OpenSTLinux by default. The default image includes Python 3.12.4, but I also need to have Python 3.11.5 available on the image. My end goal is to have both Python versions installed in a single image and ran a AI application.
- Labels:
-
OP-TEE
-
OpenSTLinux
-
STM32MP15 Lines
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2025-03-26 1:50 AM
Hi @AbhijithKannan ,
To have Python 3.11.5 available on the image (while keeping Python 3.12.4), I could suggest two ways:
* Using the OpenSTLinux SDK form the developer package (https://wiki.st.com/stm32mpu/wiki/STM32MPU_Developer_Package) to build Python 3.11.5 from its source code (https://wiki.st.com/stm32mpu/wiki/How_to_cross-compile_with_the_Developer_Package). This way might be interesting to make a quick test.
* Creating a custom layer (https://wiki.st.com/stm32mpu/wiki/How_to_add_a_customer_application) in the scope of the distribution package (https://wiki.st.com/stm32mpu/wiki/STM32MPU_Distribution_Package), adding in this layer a recipe for Python 3.11.5 (it might be copied/pasted/adapted from the recipe for Python 3.12.4), and adding this new layer to the built image (for example through the local.conf file). This way might be interesting to create a “new” distribution that includes both Python versions.
Hope this information helps.
Regards,
JC.