2023-12-05 11:37 PM
Hello,
I am working on a custom board based on STM32MP157A . For USBPHYC i am referring the driver from Linux(V5.13) and some of the registers like STM32_USBPHYC_MONITOR mentioned in the driver file are missing in the reference manual (RM0436).So i just wanted to know is it the only register missing in the reference manual (or) are there any other registers missing .If yes, could you help me in finding those registers with their offset addresses and their functionality or suggest me the actual reference manual.
please find the below attached link for the driver file i am using :
https://elixir.bootlin.com/linux/v5.13/source/drivers/phy/st/phy-stm32-usbphyc.c
Thanks&Regards,
Srikanth.
Solved! Go to Solution.
2023-12-07 8:13 AM
Hi @Srikanth1
those has already been answered in https://community.st.com/t5/stm32-mpus-products/usb-phy-issue-in-stm32mp157a/m-p/616874/highlight/true#M10576
USBPHYC_MONITOR definition could be found in RM0475 (same PHY in STM32MP13)
NO other missing registers.
Linux kernel 5.13 was never supported. We recommend to use USB drivers (Linux kernel LTS 6.1) from latest STM32MP1 Ecosystem.
Regards.
2023-12-07 4:13 AM
Hello @picasooapp321 ,
I am actually following the same approach you have mentioned and could you refer me some other ways that could help me in moving forward with USB and its Driver development
Thanks & Regards,
Srikanth.
2023-12-07 8:13 AM
Hi @Srikanth1
those has already been answered in https://community.st.com/t5/stm32-mpus-products/usb-phy-issue-in-stm32mp157a/m-p/616874/highlight/true#M10576
USBPHYC_MONITOR definition could be found in RM0475 (same PHY in STM32MP13)
NO other missing registers.
Linux kernel 5.13 was never supported. We recommend to use USB drivers (Linux kernel LTS 6.1) from latest STM32MP1 Ecosystem.
Regards.